The SNE series network engines are the most recent family of network engines in the Metasys building automation system portfolio.
Figure 1. SNE series network engines
The following table outlines the SNE models in more detail. The letter G in a model's product code indicates that the model is the Buy American version.
Features | SNE2200x-0 SNE22002-0G 1 |
SNE1100x-0 | SNE1050x-0 | SNE110Lx-0 2 |
---|---|---|---|---|
Communication interfaces |
|
|
||
Maximum number of child engines when acting as a Site Director | 3 | 2 | 2 | 0 |
Maximum allowed devices across all integrations. For example, MS/TP+IP. Includes VND integrations and devices brought in through routers. | 600 | 150 | 60 | 110 |
BACnet/IP maximum trunks 4 , 5 | 2 | 2 | 2 | 2 |
BACnet/IP maximum devices per trunk | 200 | 100 | 50 | 10 |
BACnet/SC maximum trunks 5 | 1 | 1 | 1 | 1 |
BACnet/SC maximum devices per trunk 6 | 150 | 100 | 50 | 10 |
BACnet MS/TP maximum trunks | 2 | 1 | 1 | 1 |
BACnet MS/TP maximum devices per trunk
(Johnson Controls devices only) Note: A repeater is
required if more than 50 Johnson Controls devices are on the same
trunk.
|
100 | 100 | 50 | 100 |
BACnet MS/TP maximum devices per trunk
(with third party) Note: A repeater is required if
more than 32 devices are on the same trunk and some are third
party.
|
64 | 64 | 50 | 64 |
N2 maximum trunks | 2 | 1 | 1 | n/a |
Mapped N2 devices per trunk Note: A repeater is required if more than 50 devices
are on the same trunk.
|
100 | 100 | 50 | n/a |
LonWorks maximum trunks | 1 | 1 | 1 | n/a |
LonWorks maximum devices | 255 | 127 | 60 | n/a |
Remote Field Bus maximum trunks | 6 | 3 | 3 | n/a |
Remote Field Bus maximum Johnson Controls Devices per bus | 32 | 32 | 32 | n/a |
Remote Field Bus maximum devices per bus (with third-party devices) | 16 | 16 | 16 | n/a |
Maximum objects in device 7 | 5000 | 2500 | 2500 | 2500 |
Supported type of parent server |
|
|
|
ADS-Lite-A only |
Supported integrations |
|
|||
Operating system | Wind River® Linux LTS 19 (LTS=long-term support) | |||
Microprocessor | NXP i.MX6 DualLite processor | |||
Memory | Flash 2GB of DDR3 RAM and 16 GB of eMMC Flash | |||
User interface | Metasys UI |
1 The letter G in a model's product code
indicates that the model is the Buy American version.
2 These models are intended for
use with the ADS-Lite-A servers (only) in Australia, China, Hong
Kong, India, Indonesia, Japan, Korea, Malaysia, New Zealand,
Philippines, Singapore, Taiwan, Thailand, Vietnam, and select
branches within regions of Africa and the Middle East.
3 Only the supported USB integration adapters
function with the SNE. Other integration adapters that are
not supported cannot function with the SNE.
4 Two Ethernet device connections include one
integral Ethernet port and the USB-to-Ethernet adapter,
ACC-USBETH-0, as the second Ethernet port. BACnet/SC is not
supported at this time. The second BACnet/IP trunk is supported only
at Release 13.0 and later.
5 Direct Ethernet
connection only. USB-to-Ethernet adapter does not support BACnet/SC
at this time.
6 Multiple IP integrations can be on an engine, including BACnet/IP
and BACnet/SC, but this is limited by the maximum devices that you
can map to a trunk. The total number of BACnet/IP or BACnet/SC
devices that you can map is 150. You cannot map 150 IP and 150 SC
devices at the same time because they use the same BACnet
Integration object.
7 Suggested object limit for performance
considerations.