Network engines - Metasys - LIT-1201526 - General System Information - Metasys System - 14.0

Metasys System Product Bulletin

Product
Building Automation Systems > Building Automation Systems > Metasys System
Document type
Product Bulletin
Document number
LIT-1201526
Version
14.0
Revision date
2024-09-17
Product status
Active
Metasys network engines provide network management and system-wide control coordination over one or more networks of equipment controllers, including the following:
  • Metasys CG series, CV series, FAC, FEC, VMA, TEC, and LN series equipment controllers
  • Metasys CGE, CVE, FAC, and VMA IP equipment controllers using several different topologies
  • Legacy Metasys controllers, such as UNTs, VMA14xx, and DX-9100s
  • Third-party devices

Metasys network engines may also be networked together for scaling up on large projects, and they may be networked with a Metasys Server for additional functionality and site unification. From Release 12.0, the SNE and SNC models can act as a Primary Hub, Failover Hub, or Node in the BACnet/SC network.

For more information, refer to the M4-SNE/M4-SNC Product Bulletin (LIT-12013296) .