The licensable Server IP Controller Integration feature enables a direct connection of ADS/ADX servers to IP controllers (and other devices on the IP integration, such as an IP meter or VRF) without the addition of an engine. Use the Server IP Controller Integration license packs to enable the direct connection of IP controllers to an ADS or ADX, with up to a maximum of 800 IP controllers. License packs are available in quantities of 10, 25, 100, or 200 devices.