From Metasys Release 14.0, the Energy Dashboard and Reporting feature is available as a trial license only on ADS and ADX servers. Energy Dashboard and Reporting provides real-time energy consumption and production details of various energy meter points configured in your system. Use the Energy Dashboard to access a series of energy widgets and analyze the energy use for your Metasys site. For information on Energy Dashboard and Reporting, refer to the Metasys UI Energy Dashboard and Reporting Feature User Guide (LIT-12014450) .