The Metasys system LN Series controllers use the LonWorks communication protocol and can be programmed using any compliant software, such as LN Builder. The plug-in for these devices features a graphical control logic interface that is custom-made to suit various control requirements.
LN Series controllers are fully programmable to monitor, control, and integrate a wide variety of HVAC and other building equipment, such as rooftop units, fan coils, heat pumps, unit ventilators, VAV boxes, multistage air handling units, chillers, boilers, and refrigeration systems.