Sensor/Actuator (SA) Bus - Metasys - LIT-1201526 - General System Information - Metasys System - 14.0

Metasys System Product Bulletin

Product
Building Automation Systems > Building Automation Systems > Metasys System
Document type
Product Bulletin
Document number
LIT-1201526
Version
14.0
Revision date
2024-09-17
Product status
Active

In addition to their onboard I/O interfaces, the CG, CV, and FEC family equipment controllers feature a Sensor/Actuator (SA) Bus to gain additional input and output interfaces and to connect to networked end devices. SA Bus devices include:

  • Input/Output Expansion Modules (XPMs and IOMs): add additional input and output interfaces to an equipment controller to aid in operating large or complex equipment (such as central plants or large air handlers).
  • Wired and Wireless Network Sensors: measure temperature, humidity, CO2, and occupancy, and transmit this information to the equipment controller. Various mounting options are available, including wall-mountable and duct-mountable sensors. Wireless sensors require a wireless one-to-one receiver to be connected into the SA Bus of the field controller.
  • Variable Speed Drives (VSDs): control fan and pump speed, and can be controlled directly by the equipment controller over the SA Bus.