Onboard control logic - Metasys - LIT-1201526 - General System Information - Metasys System - 14.0

Metasys System Product Bulletin

Product
Building Automation Systems > Building Automation Systems > Metasys System
Document type
Product Bulletin
Document number
LIT-1201526
Version
14.0
Revision date
2024-09-17
Product status
Active

The control logic in the equipment controllers is fully programmable, making these controllers well-suited for controlling a wide variety of equipment. The equipment controllers feature advanced logic capabilities including:

  • State-Based Control Logic: ensures the execution of only the specific control logic for any given state. State-based logic prevents energy-wasting control situations such as simultaneous heating and cooling.
  • Continuous Adaptive Control Algorithms: provide better control over time by automatically adjusting tuning parameters in response to seasonal and other load changes.