Field Controller (FC) Bus - Metasys - LIT-1201526 - General System Information - Metasys System - 14.0

Metasys System Product Bulletin

Product
Building Automation Systems > Building Automation Systems > Metasys System
Document type
Product Bulletin
Document number
LIT-1201526
Version
14.0
Revision date
2024-09-17
Product status
Active

The CG/CV and FEC MS/TP family equipment controllers feature a Field Controller (FC) Bus to share information peer-to-peer and with other components of the Metasys system. The FC Bus also allows network engines to supervise the equipment controllers.