Metasys equipment controllers directly monitor and operate the HVAC and other building system equipment using onboard inputs and outputs and locally processed control logic.
Metasys equipment controllers include multiple families of
controllers:
- FAC/FEC/VMA series equipment controllers, which were first introduced at MSEA Release 2.1, and have since been expanded and enhanced over several releases.
- CG/CV series equipment controllers, which were first introduced at Release 10.0, and succeed the FAC/FEC/VMA series (CG series and CV series equipment controllers).
- TEC3000 Thermostat controller family (TEC3000 Networked Thermostat Controllers).
- LN Series LonWorks® Controller family (LN Series LonWorks Controllers).