The Metasys system architecture is a distributed architecture. This means that the system components can be located as closely as possible to the equipment they are controlling, to provide optimum performance and reliability.
The distributed Metasys components with their data sources and the
equipment they control are connected by:
- direct wiring
- network wiring
- wireless networking
The distributed Metasys components and various connection methods ensure system-wide data sharing, coordination, and remote access.