User Management - Metasys - LIT-1201526 - General System Information - Metasys System - 13.0.50

Metasys System Product Bulletin

Product
Building Automation Systems > Building Automation Systems > Metasys System
Document type
Product Bulletin
Document number
LIT-1201526
Version
13.0.50
Revision date
2024-01-23
Product status
Active

The User Management feature facilitates the creation and management of users and their roles, category-based permissions, and privileges. Administrators can create and manage user details for Active Directory and Metasys local users. From Release 11.0, Active Directory includes Microsoft® Active Directory Federation Services (ADFS), including two-factor authentication (2FA) when the ADFS Server is configured for 2FA. This single sign-on solution helps prevent unauthorized access to Metasys, which, if not prevented, could result in data, financial, and reputational loss, system disruption, and other negative consequences.