Intuitive navigation - Metasys - LIT-1201526 - General System Information - Metasys System - 13.0.50

Metasys System Product Bulletin

Product
Building Automation Systems > Building Automation Systems > Metasys System
Document type
Product Bulletin
Document number
LIT-1201526
Version
13.0.50
Revision date
2024-01-23
Product status
Active

The Metasys UI provides the following methods for operators to find information easily and quickly about their system:

  • Spaces Tree is a set of links to each Space Dashboard. These links are intuitively organized by the site's physical hierarchy.
  • Building Network Tree provides access to objects using an alternative navigation tree to the Spaces tree.
  • Bookmarking provides a way for operators to quickly access favorite or most-frequently visited dashboards simply by bookmarking each location in the browser.
  • Search Bar enables you to quickly access specific dashboards by entering the first few letters of the name of the space or equipment.
  • Views enables you to select and use any of the user navigation trees that are assigned to you which may include Tailored Summaries. Tailored summaries display user-defined tables of system data.