SNE series network engines - Metasys - LIT-1201526 - General System Information - Metasys System - 13.0.50

Metasys System Product Bulletin

Product
Building Automation Systems > Building Automation Systems > Metasys System
Document type
Product Bulletin
Document number
LIT-1201526
Version
13.0.50
Revision date
2024-01-23
Product status
Active
Note: The firmware version for SNE series network engines is Release 13.0.1 with Metasys Release 13.0.50.

The SNE series network engines are the most recent family of network engines in the Metasys building automation system portfolio.

Figure 1. SNE series network engines

The following table outlines the SNE models in more detail. The letter G in a model's product code indicates that the model is the Buy American version.

Table 1. SNE series network engine details: SNE2200x, SNE1100x, SNE1050x, SNE110Lx
Features SNE2200x-0

SNE22002-0G 1

SNE1100x-0 SNE1050x-0 SNE110Lx-0 2
Communication interfaces
  • 1 Ethernet port 3
  • 2 RS-485 ports
  • 2 USB ports 4
  • 1 Ethernet port3
  • 1 RS-485 port
  • 2 USB ports4
Maximum number of child engines when acting as a Site Director 3 2 2 0
Maximum allowed devices across all integrations. For example, MS/TP+IP. Includes VND integrations and devices brought in through routers. 600 150 60 110
BACnet/IP maximum trunks 5 , 6 2 2 2 2
BACnet/IP maximum devices per trunk 200 100 50 10
BACnet/SC maximum trunks 6 1 1 1 1
BACnet/SC maximum devices per trunk 7 150 100 50 10
BACnet MS/TP maximum trunks 2 1 1 1
BACnet MS/TP maximum devices per trunk (Johnson Controls devices only)
Note: A repeater is required if more than 50 Johnson Controls devices are on the same trunk.
100 100 50 100
BACnet MS/TP maximum devices per trunk (with third party)
Note: A repeater is required if more than 32 devices are on the same trunk and some are third party.
64 64 50 64
N2 maximum trunks 2 1 1 N/A
Mapped N2 devices per trunk
Note: A repeater is required if more than 50 devices are on the same trunk.
100 100 50 N/A
LonWorks maximum trunks 1 1 1 N/A
LonWorks maximum devices 255 127 60 N/A
Remote Field Bus maximum trunks 6 3 3 N/A
Remote Field Bus maximum Johnson Controls Devices per bus 32 32 32 N/A
Remote Field Bus maximum devices per bus (with third-party devices) 16 16 16 N/A
Maximum objects in device 8 5000 2500 2500 2500
Supported type of parent server
  • ADS
  • ADX
  • OAS
  • ADS
  • ADX
  • ADS-Lite-E
  • OAS
  • ADS
  • ADX
  • ADS-Lite-E
  • OAS
ADS-Lite-A only
Supported integrations
  • BACnet/SC
  • BACnet/IP
    • Simplex® Fire Alarm Control Unit (FACU)
    • Cree® SmartCast® Lighting Control
    • Molex® Lighting Control
  • BACnet MS/TP Field Controller (FC) Bus
  • N2 Bus
    Note: The M4-SNE110Lx-0 model does not support the N2 Bus.
  • LonWorks® (requires USB to LON adapter)
    Note: The M4-SNE110Lx-0 model does not support the LonWorks network interface.
  • Modbus: Modbus TCP/IP on Ethernet and Modbus Remote Terminal Unit on RS-485
  • KNX IP
  • M-Bus
  • Tyco® C•CURE® 9000 and victor® Video Management
  • Zettler® Fire Panel with RS-232 adapter
  • OPC Unified Architecture (OPC UA)
  • MQ Telemetry Transport (MQTT)
Operating system Wind River® Linux LTS 19 (LTS=long-term support)
Microprocessor NXP i.MX6 DualLite processor
Memory Flash 2GB of DDR3 RAM and 16 GB of eMMC Flash
User interface Metasys UI
1 The letter G in a model's product code indicates that the model is the Buy American version.
2 These models are intended for use with the ADS-Lite-A servers (only) in Australia, China, Hong Kong, India, Indonesia, Japan, Korea, Malaysia, New Zealand, Philippines, Singapore, Taiwan, Thailand, Vietnam, and select branches within regions of Africa and the Middle East.
3 Second Ethernet port available with use of the ACC-USBETH-0 adapter.
4 Only the supported USB integration adapters function with the SNE. Other integration adapters that are not supported cannot function with the SNE.
5 Two Ethernet device connections include one integral Ethernet port and the USB to Ethernet adapter, ACC-USBETH-0, as the second Ethernet port. BACnet/SC is not supported at this time. The second BACnet/IP trunk is supported only at Release 13.0 and later.
6 Direct Ethernet connection only. USB to Ethernet adapter does not support BACnet/SC at this time.
7 Multiple IP integrations can be on an engine, including BACnet/IP and BACnet/SC, but this is limited by the maximum devices that can be mapped to a trunk. The total number of BACnet/IP or BACnet/SC devices that you can map is 150. You cannot map 150 IP and 150 SC devices at the same time because they use the same BACnet Integration object.
8 Suggested object limit for performance considerations.