Site unification - Metasys - LIT-1201526 - General System Information - Metasys System - 13.0.50

Metasys System Product Bulletin

Product
Building Automation Systems > Building Automation Systems > Metasys System
Document type
Product Bulletin
Document number
LIT-1201526
Version
13.0.50
Revision date
2024-01-23
Product status
Active

Metasys network engines can network together for scaling up on large projects. When the number of Network Engines becomes larger than a single network engine can efficiently handle as the Site Director, you can add a Metasys Server as the Site Director to unify the system.

The Metasys Server connects to the network engines over the Ethernet IP network and coordinates access to the system for all users. You can use a VPN over a WAN for communication to devices in other buildings or on remote sites; access remote sites over the Internet and an ISP, or by leased line or dial-up service using Remote Access Service (RAS) or the Point-to-Point Protocol (PPP).