Metasys Export Utility - Metasys - LIT-1201526 - General System Information - Metasys System - 13.0.50

Metasys System Product Bulletin

Product
Building Automation Systems > Building Automation Systems > Metasys System
Document type
Product Bulletin
Document number
LIT-1201526
Version
13.0.50
Revision date
2024-01-23
Product status
Active
The Metasys Export Utility extracts historical trend, alarm, and audit data from the Network Engine or ADS/ADX. This data is then provided in several file formats, such as Microsoft Excel® spreadsheet (.xls) and Access® database (.mdb). You can instantly extract the selected data or schedule an extraction at a convenient time or interval.
Note: Metasys Export Utility is not supported for the Open Application Server (OAS).