Historical data storage and management - Metasys - LIT-1201526 - General System Information - Metasys System - 13.0.50

Metasys System Product Bulletin

Product
Building Automation Systems > Building Automation Systems > Metasys System
Document type
Product Bulletin
Document number
LIT-1201526
Version
13.0.50
Revision date
2024-01-23
Product status
Active

A Metasys Server can be added to the Metasys system when the long-term historical data storage needs exceed the capacity of a network engine. The Metasys Server connects to the network engines over the Ethernet IP network and offers manual, scheduled, and automatic archiving of historical data, including trend data, event messages, operator transactions, and system configuration data. See Server comparison to understand the archiving capabilities of each Metasys Server type.

Metasys operators can view up to five years' worth of data within Metasys UI. This feature helps operators identify opportunities for system performance improvements and energy savings by providing year-over-year energy reporting.
Note: This feature requires the Metasys Historical Data Add-on license for an OAS, which needs to be purchased separately.