Advanced Reporting - Metasys - LIT-1201526 - General System Information - Metasys System - 13.0.50

Metasys System Product Bulletin

Product
Building Automation Systems > Building Automation Systems > Metasys System
Document type
Product Bulletin
Document number
LIT-1201526
Version
13.0.50
Revision date
2024-01-23
Product status
Active

The Metasys Advanced Reporting System is an optional feature of the ADX that provides historical and configuration data reporting capabilities separate from those available in the SMP.

Metasys Advanced Reporting System allows authorized users to run reports to review the configuration and performance of the Metasys system. Users can easily view these reports in a web browser.

The following reports are available for the points included in the reporting system user views:

  • Configuration Setup Review
  • System Behavior
  • Trend Report—statistical calculations and Mean Kinetic Temperature (MKT)
  • Trend Detail Report—summary data

You can export a report and save it in a variety of formats, such as Microsoft Excel or PDF, for later use.

For information about the reporting capabilities offered by the Metasys UI, see Advanced Search and Reporting.