Metasys Server - Metasys - LIT-1201526 - General System Information - Metasys System - 13.0.50

Metasys System Product Bulletin

Brand
Metasys
Product name
Metasys System
Document type
Product Bulletin
Document number
LIT-1201526
Version
13.0.50
Revision date
2024-01-23
Product status
Active
Language
English

The Metasys Server is an optional component that can be added to the Metasys system. The Server manages the collection and presentation of large amounts of trend data, event messages, operator transactions, and system configuration data, and provides one or more of the following:

  • Site unification
  • Long-term, large-scale storage of historical data
  • Advanced reporting
  • Metasys UI, an intuitive user interface
  • SMP user interface, which provides advanced operation and system navigation tree to show a hierarchical network view of the entire system for all connected devices

The ADS, ADX, and OAS support BACnet/SC and can act as a Primary Hub or Failover Hub in the BACnet/SC network topology. You need to purchase the M4-BACNETSC-0 add-on license to use BACnet/SC. For more information about BACnet/SC, refer to BACnet/SC Workflow Technical Bulletin (LIT-12013959) .