LN Series LonWorks Controllers - Metasys - LIT-1201526 - General System Information - Metasys System - 13.0.50

Metasys System Product Bulletin

Product
Building Automation Systems > Building Automation Systems > Metasys System
Document type
Product Bulletin
Document number
LIT-1201526
Version
13.0.50
Revision date
2024-01-23
Product status
Active

The Metasys system LN Series controllers use the LonWorks communication protocol and can be programmed using any compliant software, such as LN Builder. The plug-in for these devices features a graphical control logic interface that is custom-made to suit various control requirements.

LN Series controllers are fully programmable to monitor, control, and integrate a wide variety of HVAC and other building equipment, such as rooftop units, fan coils, heat pumps, unit ventilators, VAV boxes, multistage air handling units, chillers, boilers, and refrigeration systems.