Distributed - Metasys - LIT-1201526 - General System Information - Metasys System - 13.0.50

Metasys System Product Bulletin

Product
Building Automation Systems > Building Automation Systems > Metasys System
Document type
Product Bulletin
Document number
LIT-1201526
Version
13.0.50
Revision date
2024-01-23
Product status
Active

The Metasys system architecture is a distributed architecture. This means that the system components can be located as closely as possible to the equipment they are controlling, to provide optimum performance and reliability.

The distributed Metasys components with their data sources and the equipment they control are connected by:
  • direct wiring
  • network wiring
  • wireless networking

The distributed Metasys components and various connection methods ensure system-wide data sharing, coordination, and remote access.