Application and Data Server Lite system requirements - Metasys - LIT-12011832 - General System Information - Metasys System - 13.0.50

Metasys System Configuration Guide

Product
Building Automation Systems > Building Automation Systems > Metasys System
Document number
LIT-12011832
Version
13.0.50
Revision date
2024-12-02
Product status
Active
Table 1. Application and Data Server Lite system requirements

Recommended computer platform 1

Intel i7 processor latest version with at least 6 cores or better

2 x 500 GB hard disk (RAID 1) 2 with 40 GB free space after installation of all prerequisite software and before installation of ADS-Lite software. Configure RAID 1 (mirroring) with disk write-caching turned on.
Note: Prerequisite software includes the supported operating system, database software, .NET Framework, and any other software or service packs required for your ADS configuration.

Graphics adapter (1 GB RAM, ATI® Technologies or NVIDIA® Corporation, 64-bit compatible [for 64-bit operating systems], Small Form Factor [SFF] if required)

Required minimum memory 3

16 GB RAM

The VM host must have the 16 GB recommended RAM at all times. When you configure the VM, do not select the enable dynamic memory option.

Supported operating systems and database software 4

Windows® 11 Pro and Windows® 11 Enterprise versions 22H2, 21H2 (64-bit) General Availability Channel (GAC)

Windows® 10 Pro and Windows 10 Enterprise Editions versions 21H2, 22H2 (64-bit).

Windows® 10 Enterprise LTSC (1809, 21H2) (64-bit)
Database software:
  • SQL Server® 2022 Express with CU9 (64-bit)
  • SQL Server® 2019 Express with CU18 (64-bit)
    Note: SQL Server 2019 or later may cause the configuration service cache that builds stored procedures to time out. This causes the user's logon to Metasys UI to fail. To resolve this issue, set SQL Server 2019 or later databases to run in 2017 compatibility mode. For more information, refer to docs.microsoft.com
  • SQL Server® 2017 Express with CU31 (64-bit)

Supported operating systems for Metasys client devices

Windows® 11 Pro and Windows® 11 Enterprise versions 22H2, 21H2 (64-bit) General Availability Channel (GAC)

Windows® 10 Pro and Windows 10 Enterprise Editions versions 21H2, 22H2 (64-bit).

Apple® macOS® 11 Big Sur

Apple® macOS® 12 Monterey

Apple® macOS® Ventura 13.2

Notes:
  • In OS X, you cannot view Graphics+ graphics in the Site Management Portal UI.
  • Apple operating systems are supported for Metasys client computers only.

Supported web browser software for Metasys Site Management Portal client

Microsoft® Edge® version 119 or later

Apple® Safari® 15.0 or later

Note: Other browsers, such as Mozilla® Firefox®, may also be used but are not fully supported. You use the web browser to download the Launcher application. After you install the Launcher application, you use the Launcher, not the web browser, to log in to the Site Management Portal (SMP) user interface.

Supported web browser software for Metasys UI clients

Microsoft® Edge® version 119 or later

Google® Chrome™ version 119 or later
Note: Metasys UI does not support incognito mode. To exit incognito mode, click or tap the X icon of the browser window or tab and then open a new browser window or tab. For more information on incognito mode in Google Chrome, click here.
Apple® Safari® 15.0 or later
Note: Metasys UI does not support private browsing. To exit private browsing, click or tap Private in the browser window.

Supported virtual environments

Microsoft Hyper-V™

VMware®

Supported user interfaces

Metasys UI

Site Management Portal (SMP)

Note: SMP requires a license and is available only to existing Metasys customers. If you licensed SMP at an earlier release, you can use the same license after you upgrade to a later release.
Additional software included with the ADS Lite software download

Microsoft .NET Framework 4.7.2

Microsoft .NET 6.0.16

Launcher Software

RabbitMQ Server 3.8.16

Erlang OTP 23.2 (11.1.4)

Optional hardware

Any network or local printer supported by the qualified Windows operating system

Optional software

CCT Software

SCT Software

Metasys Database Manager

Metasys Export Utility

1 Our computer platform and memory recommendations are not meant to imply that older or slower machines are not usable. Refer to the Network and IT Guidance Technical Bulletin (LIT-12011279) 1 for more information regarding computer/server recommendations.
2 For best performance, use Serial Attached SCSI (SAS) hard drives, not Small Computer System Interface (SCSI) hard drives.
3 It is recommended to use RAM that the computer supports.
4 Refer to the Network and IT Guidance Technical Bulletin (LIT-12011279) for specific Microsoft Windows operating system settings that may be required for your Metasys system configuration.