System Configuration Tool Pro (SCT Pro) - Metasys - LIT-12011832 - General System Information - Metasys System - 13.0.50

Metasys System Configuration Guide

Product
Building Automation Systems > Building Automation Systems > Metasys System
Document type
Configuration Guide
Document number
LIT-12011832
Version
13.0.50
Revision date
2024-12-02
Product status
Active

SCT Pro is a modernized version of SCT that runs in the browser and does not require the Launcher. SCT Pro provides significantly streamlined workflows, and greatly simplifies tasks that were previously time consuming or cumbersome. For example, you can use SCT Pro to maintain healthy backup practices for a site, such as setting up backups to occur automatically on a recurring schedule.

When you install SCT, you also have access to the SCT Pro web application. You can launch the HTML user interface from SCT or from a URL on any client device type (workstation, tablet, or phone).

SCT Pro currently includes a subset of the features that are available in SCT. With each release, features from SCT are incorporated into SCT Pro and optimized to significantly streamline workflows and simplify tasks. For example, SCT Pro features a single, automated process to upgrade network engines. SCT Pro also includes features that are not available in SCT. For a summary of the main differences between SCT and SCT Pro, refer to the System Configuration Tool Catalog Page (LIT-1900198) .

SCT and SCT Pro use the same databases and share the same job scheduling system, named the Action Queue. You can use SCT and SCT Pro interchangeably and select the most appropriate application for the current task.

Use SCT Pro to complete any of the following tasks:
  • Provision a new network engine
  • Upload and download a site
  • Perform a backup of a site
  • Schedule automatic recurring backups
  • Restore a site from a backup
  • Upgrade a device
  • Discover devices on the same subnet as the SCT Pro server
The following table describes which specific tools and capabilities are most appropriate for each type of network engine:
Table 1. Network Engine Re-imaging Tools
Tools to use NAE35, NAE45, NCE25, NAE55 NAE35, NAE45, NCE25 NAE55 SNE, SNC
Release 9.0 Windows Release 9.0.7 or later Linux Release 10.0, 10.1, 11.0, or 12.0 Linux Release 10.1, 11.0, 12.0, or 13.0 Linux
NAE Update Tool 1 X X X
SCT 16.0 X X X
SCT Pro 16.0 X X X X

For a guided tour of features on a particular page in SCT Pro, click on your account name in the upper-right corner of the SCT Pro window, and then click Tour.

For more information about SCT Pro, refer to SCT Pro Help (LIT-12013035).

1 The NAE Update Tool continues to be a component of the SCT install. However, we encourage you to work with SCT Pro instead of the NAE Update Tool.