Use the following table to help you determine the ADS/ADX user product that you need to order. The table provides examples of the total number of supported users who can be simultaneously logged on the SMP and Metasys UI.
| Metasys Server type | Examples of Metasys Server concurrent users | |
|---|---|---|
| SMP UI | Metasys UI | |
|
5-user ADS/ADS-Lite/OAS |
0 | 5 |
| 2 | 3 | |
| 5 | 0 | |
| 10-user ADX | 0 | 10 |
| 5 | 5 | |
| 8 | 2 | |
| 10 | 0 | |
| 25-user ADX | 0 | 25 |
| 10 | 15 | |
| 20 | 5 | |
| 25 | 0 | |
| 50-user ADX | 0 | 50 |
| 10 | 40 | |
| 25 | 25 | |
| 50 | 0 | |
| 100-user ADX | 5 | 50 1 |
| 10 | 501 | |
| 25 | 501 | |
| 50 | 501 | |
| 75 | 25 | |
| 100 | 0 | |
For example, as shown in Table 1, with a 5-user ADS or ADS-Lite, 5 Metasys UI users are supported if no SMP users are logged in, or 3 Metasys UI users are supported if 2 SMP users are logged in. Similarly, with a 50-user ADX, 50 Metasys UI users are supported if no SMP users are logged in, or 40 Metasys UI users are supported if 10 SMP users are logged in. The only Metasys UI user restriction applies to a 100-user ADX: no more than 50 Metasys UI users are supported, regardless of the number of SMP users.