Metasys Advanced Reporting System - Metasys - LIT-12011832 - General System Information - Metasys System - 13.0.50

Metasys System Configuration Guide

Product
Building Automation Systems > Building Automation Systems > Metasys System
Document number
LIT-12011832
Version
13.0.50
Revision date
2024-12-02
Product status
Active

The Metasys Advanced Reporting System is a standard capability of all ADX servers when using supported SQL Server software, with SQL Server Reporting Services (SSRS) installed. The web-based reporting interface provides standard report sets. You can review the alarm and trend configuration of your site, run summary and detail reports to monitor alarm and event information, view offline information, combine alarm and audit information in a single report, and provide summary and detailed trend aggregations. The site’s All Items or User View navigation tree filters the report information. You can customize the date range and data type for each report. When a report is created in the user interface, you can export the data into common applications, such as Microsoft Excel® spreadsheet or Adobe® PDF formats.

For information about the reporting capabilities offered by the Metasys UI, refer to Metasys UI Help (LIT-12011953) .