Site Director limitations and recommendations - Metasys - LIT-12011832 - General System Information - Metasys System - 13.0.50

Metasys System Configuration Guide

Product
Building Automation Systems > Building Automation Systems > Metasys System
Document type
Configuration Guide
Document number
LIT-12011832
Version
13.0.50
Revision date
2024-12-02
Product status
Active

The following tables describe performance guidelines and limitations of the Metasys system Site Directors.

Note: To take advantage of encrypted communications, upgrade the Site Director to the latest Metasys release for its type. For best performance also upgrade the network engines to the newer release. Network engines at Release 5.2 or later function with Release 13.0, but to ensure best performance, upgrade engines to newer versions as soon as it is practical.
Table 1. Engine Site Director limitations and recommendations
Maximum allowed Type of Site Director

NAE35

SNE1050x

NAE45

SNE1100x

NAE55

SNE2200x

NAE85

LCS85

NCE25

SNC replacements of NCE25 1

Total engines 3 3 4 4 1 2
Simultaneous Metasys UI users 3 2 4 24 44 10 5 24
Simultaneous SMP users 6 2 7 27 47 10 8 27
Objects in device 9 2,500 2,500 5,000 25,000 10 2,500
Objects in a single folder 700 700 700 700 700
Dynamic values per graphics 100
Results displayed in a global search 500
Languages 1 1 1 18 11 1
Characters in the name of an object 400
Characters in the description of an object 64
Nesting levels for object creation 7
Extensions per object 10
Sets for third-party BACnet states text 1,000
Characters for a third-party BACnet states text 60
Members for a multi-value third-party BACnet states text 500
Non-Simultaneous SMP users Limited only by memory capacity
SMP user views Limited only by memory capacity
Simultaneous browsers per client computer 2 (mix of online and SCT)
DLLR load extension Limited only by memory capacity. If you plan to attach a large number of load extensions to a single DLLR object, consider the memory limitation. For load extensions attached to one DLLR object, there is a 64 KB text limit for the list of the Loads fully qualified references. Load Limit = (64 x 1024)/average number of characters per load. 1024 Bytes equals 1 KB. For example, if your DLLR object is configured with Loads that have fully qualified references that average 100 characters (including dots) in length, then you can support approximately 650 loads (64 x 1024/100) for that DLLR. If you reach the memory limit, you may need to combine loads. For example, if a site has multiple physical meters, split the meters across multiple controllers and apply appropriate DLLR loads, if possible. Otherwise, use Interlock or Multiple Command objects to reduce the number of loads added to the DLLR.
DLLR objects Limited only by memory capacity.
Table 2. Server Site Director limitations and recommendations
Maximum allowed

Type of Site Director

ADS Desktop ADS-Lite-E 12 ADS-Lite-A 13 ADX OAS
Total engines 14 14 5 15 4 16 1,000 17 OASMIN: 0

OASSTD: up to two

Simultaneous Metasys UI users 18 5 5 5 25/50 5
Simultaneous SMP users 19 5 5 5 10/25/

50/100 20

5
Dynamic values per graphics 100
Results displayed in a global search 2,000
Languages 18
Objects in entire system 3 million/ 750k (for ADX Site Director Only)
Objects in device 21 Limited by SQL Server storage capacity 20,000
Objects in a single folder 700
Characters in the name of an object 400
Characters in the description of an object 64
Nesting levels for object creation 7
Extensions per object 10
Sets for third-party BACnet states text 1,000
Characters for a third-party BACnet states text 60
Members for a multi-value third-party BACnet states text 500

Non-Simultaneous users

Limited only by memory capacity

User views

Limited only by memory capacity
Simultaneous browsers per client computer 22 2 (Mix of online and SCT)
DLLR load extension Limited only by memory capacity. If you plan to attach a large number of load extensions to a single DLLR object, consider the memory limitation. For load extensions attached to one DLLR object, there is a 64 KB text limit for the list of the Loads fully qualified references. Load Limit = (64 x 1024)/average number of characters per load. 1024 Bytes equals 1 KB. For example, if your DLLR object is configured with Loads that have fully qualified references that average 100 characters (including dots) in length, then you can support approximately 650 loads (64 x 1024/100) for that DLLR. If you reach the memory limit, you may need to combine loads. For example, if a site has multiple physical meters, split the meters across multiple controllers and apply appropriate DLLR loads, if possible. Otherwise, use Interlock or Multiple Command objects to reduce the number of loads added to the DLLR.
DLLR objects Limited only by memory capacity.
Table 3. Maximum number of users supported on Metasys Server type Site Directors
Type of Metasys Server

Computer supported platform

Site Management Portal (SMP) Users (up to)

Metasys UI Users (up to)

Desktop

Server

ADS05U

Yes

-

5

5

OASSTD

Yes 23

Yes 24

5

5

OASMIN

Yes23

Yes24

5

5

ADX10U

-

Yes

10

25

ADX25U

-

Yes

25

25

ADX50U

-

Yes

50

50

ADX100U 25

-

Yes

100

50

Table 4. Maximum number of network engines supported based on Metasys Server type and Server size

Site Director with maximum users

1 to 14 engines

1 to 25 engines

1 to 50 engines

1 to 100 engines

1 to 300 engines

1 to 1,000 engines

ADS05U

ADS

         

ADX10U

 

Small ADX

Medium ADX

Medium/Large ADX

Large/Extra Large ADX

Extra Large ADX

ADX25U

Small ADX

Medium ADX

ADX50U

   

Medium/Large ADX

ADX100U

   

For ADS/ADX computer hardware requirements, refer to the Technical Specifications section of this document:

1 SNC2515x-0xx, SNC2515x-04x, SNC1612x-0xx, and SNC1612x-04x.
2 An NCE25 or SNC can only act as Site Director for itself.
3 When both SMP and Metasys UI are available for login to a device, the supported number of simultaneous Metasys UI users is reduced by any users who have logged in using SMP.
4 This NxE model does not support Metasys UI. This SNx model includes Metasys UI starting at Release 13.0.
5 Metasys UI is available on NAE85 devices at Release 12.0 and later.
6 When both SMP and Metasys UI are available for login to a device, the supported number of simultaneous SMP users is reduced by any users who have logged in using Metasys UI.
7 Prior to Release 13.0, these device models include only SMP. From Release 13.0, this SNx device model includes only Metasys UI.
8 From Release 12.0, SMP is available on these device models for only existing customers who have purchased an SMP license.
9 Includes all points, extensions, graphics (background image), trend study, and other objects, such as schedules and interlocks.
10 The 25,000 limit applies only when the 15K Upgrade is licensed for the NAE85/LCS85. The limit is 10,000 without the 15K Upgrade license.
11 From Release 12.0, NAE85/LCS85 support 18 languages. All other cases support a single language.
12 The ADS-Lite-E cannot host servers.
13 The ADS-Lite-A cannot host servers.
14 Varies with concurrent connection.
15 Supports up to five of the following: SNE1100x, SNE1050x, SNC2515x-0xx, SNC2515x-04x, SNC1612x-0xx, SNC1612x-04x, NAE35, NAE45, NCE25, NIE29, NIE39, and NIE49.
16 Supports up to three NAE-Lite engines and one SNE110Lx, NIE29, NIE39, and NIE49.
17 Depends on computer hardware. See the table Maximum number of network engines supported based on Metasys Server type and Server size for more information.
18 When both SMP and Metasys UI are used to login to a server, the supported number of simultaneous Metasys UI users is reduced by any users who have logged in using SMP.
19 From Release 12.0, SMP is available on servers for only MVE sites and existing customers who have purchased an SMP license. When both SMP and Metasys UI are used to login to a server, the supported number of simultaneous SMP users is reduced by any users who have logged in using Metasys UI.
20 Depends on version of ADX.
21 Includes all points, extensions, graphics (background image), trend study, and other objects, such as schedules and interlocks.
22 The number of tabs supported in your browser depends on the operating system (OS) of the Metasys device you are accessing. It can also be dependent on other active users.
23 Virtual Machine or Turnkey only.
24 Virtual Machine only.
25 Metasys for Validated Environments does not support the 100 user ADX.