SCT limitations - Metasys - LIT-12011832 - General System Information - Metasys System - 13.0.50

Metasys System Configuration Guide

Product
Building Automation Systems > Building Automation Systems > Metasys System
Document type
Configuration Guide
Document number
LIT-12011832
Version
13.0.50
Revision date
2024-12-02
Product status
Active
Table 1. SCT limitations
Description Supported Comments
Max. number of concurrently active archives 10  
Max. number of simultaneous browser tabs or connections
  • 10 with Windows Desktop OS
  • Unlimited with Windows Server OS
If additional browser tabs or connections are accessed when SCT is installed on Desktop OS, SCT does not function as expected.
Max. size of an active database or project in SCT 10 GB Using supported Microsoft SQL Server Express software.
No limit Using supported Microsoft SQL Server Standard or Datacenter Software