MS/TP performance guidelines - Metasys - LIT-12011832 - General System Information - Metasys System - 13.0.50

Metasys System Configuration Guide

Product
Building Automation Systems > Building Automation Systems > Metasys System
Document number
LIT-12011832
Version
13.0.50
Revision date
2024-12-02
Product status
Active
Table 1. MS/TP performance guidelines
Performance rating COV rate Token loop time
Low > 500 messages per minute > 3,000 ms
Medium Between 400 and 500 messages per minute Between 2,000 and 3,000 ms
High < 400 messages per minute < 2,000 ms