Vendor integrations on engines - Metasys - LIT-12011832 - General System Information - Metasys System - 13.0.50

Metasys System Configuration Guide

Product
Building Automation Systems > Building Automation Systems > Metasys System
Document type
Configuration Guide
Document number
LIT-12011832
Version
13.0.50
Revision date
2024-12-02
Product status
Active

The maximum number of simultaneous integrations supported on an engine depends on the processing capabilities of the engine's platform.

An NAE8500 or an OAS that runs on an appropriately resourced platform can simultaneously support a maximum of eight vendor-based integrations. All NAE and SNx based engines can simultaneously support a maximum of two vendor-based integrations. Embedded platforms like the NAE and the SNx based engines tend to be resource constrained, so some protocols like KNX, C•CURE-victor, OPC UA, and Zettler can be impacted if they are combined with other vendor-based integrations. Combinations like KNX + Modbus are not supported on these type of engine models and can result in unexpected behavior, if implemented. The following table shows the maximum number of simultaneous integrations that are supported on an NAE or SNx based engine.
Table 1. Maximum number of simultaneous integrations that are supported on an NAE or SNx based engine
Vendor integration type Maximum number of supported simultaneous integrations (standard protocol drivers)
MQTT 1
Modbus (TCP or RS-485) 2
M-Bus 2
KNX 1
C•CURE-victor 1
OPC Unified Architecture (UA) 1
Zettler 1