Network Engine comparison - Metasys - LIT-12011832 - General System Information - Metasys System - 13.0.50

Metasys System Configuration Guide

Product
Building Automation Systems > Building Automation Systems > Metasys System
Document type
Configuration Guide
Document number
LIT-12011832
Version
13.0.50
Revision date
2024-12-02
Product status
Active
Table 1. Network Engine Release support comparison
Model Release 9.0 Release 9.0.7 or later Release 10.0 Release 10.1 Release 11.0 Release 12.0 Release 13.0

NCE25

X X 1   Succeeded by SNC models.

NAE35, NAE45

X X 2   The SNE1050x succeeds the NAE35 series and the SNE1100x succeeds the NAE45 series.

NAE55

X   X 3 X 4 X 5 X 6 Discontinued

NAE85

X   X X X X X

NIE29, NIE39, NIE49

X X 7   Discontinued Discontinued Discontinued Discontinued

NIE59

X   X X X X Discontinued
Important: All NIEx9 models have been discontinued from manufacture, because starting at 9.0.7 and 10.0, NAE models include the integration functionality of the NIE. Existing NIE59s can be field-upgraded to 10.0, 10.1, 11.0, and 12.0 respectively.
NIE89 X   X X X X Discontinued
Important: All NIEx9 models have been discontinued from manufacture, because starting at 9.0.7 and 10.0, NAE models include the integration functionality of the NIE. Existing NIE89s can be field-upgraded to 10.0, 10.1, 11.0, and 12.0 respectively.

NIE55, NIE85

X   Discontinued Discontinued Discontinued Discontinued Discontinued
SNE       X X X X
SNC       X X X X
Table 2. Network Engine integrations available by Metasys Release
Integration Release 9.0 Release 9.0.7 or later Release 10.0 Release 10.1 Release 11.0 Release 12.0 Release 13.0
BACnet/SC           X 8 X 8
MQTT           X 9 X 9
BACnet/IP X X X X X X X
BACnet MS/TP X X X X X X X
Legacy N1 LAN X            
Legacy N2 Bus X X X X 10 X10 X 10
LonWorks X   X X 11 X11 X 11
Modbus RTU and TCP X X X X X X X
KNX IP X X X X X X X
M-Bus Serial and IP X X X X X X X
C•CURE-victor     X X X X X
Simplex Fire (secondary monitoring only)     X X X X X
Preferred Vendor Lighting Systems     X X X X X
Zettler Fire Panel       X X X X
OPC Unified Architecture (OPC UA)         X X X
WRS-RTN Wireless Supervisor X            
1 Only NCE25xx-0 is available to upgrade to Metasys 9.0.7 or later with Linux OS.
2 Only NAE35xx-2 and NAE45xx-2 are available to upgrade to Metasys 9.0.7 or later with Linux OS.
3 Only NAE55xx-2 and NAE55xx-3 are available to upgrade to Metasys 10.0 with Linux OS.
4 Only NAE55xx-2 and NAE55xx-3 are available to upgrade to Metasys 10.1 with Linux OS.
5 Only NAE55xx-2 and NAE55xx-3 are available to upgrade to Metasys 11.0 with Linux OS.
6 Only NAE55xx-3 is available to upgrade to Metasys 12.0 with Linux OS.
7 Only NIE29xx-0s, NIE39xx-2, and NIE49xx-2 are available to upgrade to Metasys 9.0.7 or later with Linux OS.
8 NAE85, NAE55xx-3, SNEs, and SNCs support BACnet/SC. NAE55xx-3 supports BACnet/SC at Release 12 only.
9 MQTT is supported only on the SNC and SNE series engines from Release 12.0.
10 The M4-SNE110Lx-0 model does not support the N2 Bus.
11 The M4-SNE110Lx-0 model does not support LonWorks.