NCE Series Network Control Engine - Metasys - LIT-12011832 - General System Information - Metasys System - 13.0.50

Metasys System Configuration Guide

Product
Building Automation Systems > Building Automation Systems > Metasys System
Document number
LIT-12011832
Version
13.0.50
Revision date
2024-12-02
Product status
Active
The NCE provides support for the same communications protocols as the NAE, but also offers the Input/Output (I/O) point connectivity and direct digital control capabilities of a Metasys Field Equipment Controller (FEC). The NCE provides a cost-effective solution designed for central plants and large built-up air handler applications. All NCE models provide IP Ethernet network connectivity, the Site Management Portal UI, and the network supervisory control functions featured on network automation engines. Depending on the model and software release, an NCE supports either a BACnet MS/TP Bus, an N2 Bus, or a LonWorks network trunk. The NCE also provides built-in support for third-party protocols, including Modbus, M-Bus, and KNX.
Note: Starting at Release 10.1, the SNC Series Network Controllers succeed the NCE Series of the Network Control Engine family. For more information about the SNC see SNC series network control engines.