NAE Series Network Automation Engine - Metasys - LIT-12011832 - General System Information - Metasys System - 13.0.50

Metasys System Configuration Guide

Product
Building Automation Systems > Building Automation Systems > Metasys System
Document type
Configuration Guide
Document number
LIT-12011832
Version
13.0.50
Revision date
2024-12-02
Product status
Active

The NAE is available with options to support various communications protocols including BACnet/SC, BACnet/IP, BACnet® MS/TP, N2 Bus, N2 over Ethernet, and LonWorks® protocol. Built-in support for third-party protocols, including Modbus, M-Bus, KNX, C•CURE-victor, and OPC UA is also included. The following model is available to upgrade:

  • The NAE85 supports large BACnet/IP integrations.

    From Release 12.0, the NAE85 supports BACnet/SC and can act as a Primary Hub, Failover Hub, or Node in the BACnet/SC network topology. You need to purchase the M4-BACNETSC-0 add-on license to use BACnet/SC. For more information about BACnet/SC, refer to BACnet/SC Workflow Technical Bulletin (LIT-12013959) .

Note: The SNE Series of Network Engines succeed the NAE Series Network Engine family. For more information about the SNE see SNE series network engines.