Network Engines - Metasys - LIT-12011832 - General System Information - Metasys System - 13.0.50

Metasys System Configuration Guide

Product
Building Automation Systems > Building Automation Systems > Metasys System
Document type
Configuration Guide
Document number
LIT-12011832
Version
13.0.50
Revision date
2024-12-02
Product status
Active

Network engines perform a key role in the Metasys system architecture. These network engines provide network management and system-wide control coordination over one or more networks of equipment controllers, including the following Metasys equipment controllers:

  • General Purpose Application MS/TP Controllers (CGMs)
  • General Purpose Application Ethernet Controllers (CGEs)
  • VAV Box MS/TP Controllers (CVMs)
  • VAV Box Ethernet Controllers (CVEs)
  • Field Equipment Controllers (FECs) and Advanced Application Field Equipment Controllers (FACs)
  • Variable Air Volume Modular Assembly (VMA) Controllers
  • Terminal Equipment Controllers (TECs)
  • LN series equipment controllers
  • Legacy Metasys controllers, such as Unitary (UNT) controllers, Variable Air Volume Assembly (VMA14xx) controllers, and DX-9100 controllers
  • Third-party equipment controllers

The network engines can be networked together for scaling up on large projects, and they can be networked with an ADS, ADX, or OAS for additional functionality and site unification.

Network engines provide building control scheduling, alarm and event management, energy management, data exchange, historical data storage and management, and custom control logic. Network engines include an embedded user interface. For system navigation and operation, use web browser connections to access the user interface. Network engines are secured from unauthorized access using password protection, permission access control, and IT security best practices.

In addition to providing general comprehensive equipment monitoring and control, network engines also offer specialized capabilities by series, model, and software release to meet a variety of application requirements. The network engines are identified by three types:

Small-capacity engines

  • Network Automation Engines: NAE35 and NAE45
    Note: The NAE35 and NAE45 are not capable of running firmware greater than Release 9.0.x.
  • SNE Series of Network Engines: SNE1050x and SNE1100x
    Note: The SNE1050x model succeeds the NAE35 model and the SNE1100x model succeeds the NAE45 model of engines.
  • Network Control Engine: NCE25
    Note: The NCE25 is not capable of running firmware greater than Release 9.0.x.
  • SNC Series of Network Control Engines: SNC2515x-0, SNC2515x-0H, SNC2515x-04, SNC2515x-04H, SNC1612x-0, SNC1612x-0H, SNC1612x-04, and SNC1612x-04H
    Note: The SNC models succeed the NCE25 models of engines.

Large-capacity engines

  • Network Automation Engine: NAE55
    Note: The NAE55 is not capable of running firmware greater than Release 12.x.
  • SNE Series of Network Engines: SNE2200x
    Note: The SNE2200x succeeds the NAE55 model of engines.

Software-only engines

  • Network Automation Engine: NAE85
  • LonWorks® Control Server: LCS85