Unified and split ADX with dual network cards - Metasys - LIT-12011832 - General System Information - Metasys System - 13.0.50

Metasys System Configuration Guide

Product
Building Automation Systems > Building Automation Systems > Metasys System
Document type
Configuration Guide
Document number
LIT-12011832
Version
13.0.50
Revision date
2024-12-02
Product status
Active

A unified or split ADX system can use computers that have more than one network card. Other Metasys software applications such as Metasys Export Utility, also support computers with multiple network cards. The steps for configuring the cards are included with the software installation instructions for the particular application. The following figure shows two examples of supported network configurations.

Figure 1. Network examples with dual network cards