Third-party network integration - Metasys - LIT-12011832 - General System Information - Metasys System - 13.0.50

Metasys System Configuration Guide

Product
Building Automation Systems > Building Automation Systems > Metasys System
Document number
LIT-12011832
Version
13.0.50
Revision date
2024-12-02
Product status
Active

The network engines offer seamless integration of Modbus, M-Bus, KNX, or other third-party network to the Metasys system. The following figure shows the SNEs and SNC integrating third-party devices. A KNX IP Gateway is also shown.

Figure 1. Third-party network integration