Multiple network engine system configuration with one network engine designated as the Site Director - Metasys - LIT-12011832 - General System Information - Metasys System - 13.0.50

Metasys System Configuration Guide

Product
Building Automation Systems > Building Automation Systems > Metasys System
Document number
LIT-12011832
Version
13.0.50
Revision date
2024-12-02
Product status
Active

To extend the capabilities of your system, add one or more additional network engines. In the following figure, one network engine designated as the Site Director provides a user interface for accessing all devices on the site. This configuration supports up to four simultaneous users.

Note:
  • This configuration only provides long-term storage of data through the use of the Metasys Export Utility installed on a computer.
  • The NAE45-Lite can be partnered with other NAE45-Lite devices only. Additionally, the NAE45-Lite requires an ADS-Lite-A Site Director, and both of these are available in specific markets only.
  • Similarly, the SNE110Lx can be partnered with other SNE110Lx type network engines only. Additionally, the SNE110Lx requires an ADS-Lite-A Site Director, and both of these are available in specific markets only.
Figure 1. Multiple network engine system configuration with one network engine designated as the Site Director