Large ADX site configuration - Metasys - LIT-12011832 - General System Information - Metasys System - 13.0.50

Metasys System Configuration Guide

Product
Building Automation Systems > Building Automation Systems > Metasys System
Document number
LIT-12011832
Version
13.0.50
Revision date
2024-12-02
Product status
Active

The ADX you select for a large site can be a 10, 25, 50, or 100-user ADX. However, Metasys UI supports a maximum of 50 users, even for a 100-user ADX, as listed in Table 3.

For more information about the technical specifications for a large ADX system, refer to the Extended Application and Data Server System Requirements (Unified ADX Systems, 50 or 100 Users) table in the Technical Specifications section of the Application and Data Server (ADS) and Extended Application and Data Server (ADX) Product Bulletin (LIT-1201525) .
Note: MVE supports the same number of users as the ADX where it is installed.