BACnet/IP network system configuration - Metasys - LIT-12011832 - General System Information - Metasys System - 13.0.50

Metasys System Configuration Guide

Product
Building Automation Systems > Building Automation Systems > Metasys System
Document type
Configuration Guide
Document number
LIT-12011832
Version
13.0.50
Revision date
2024-12-02
Product status
Active

BACnet/IP devices are connected directly to the IP Ethernet network. The network engine communicates with the devices using the BACnet protocol and presents the BACnet data to the system in the same way as the other data in the Metasys system. The following figure shows the SNE1050 integrated into the Metasys network. Other BACnet/IP devices are integrated in the same way.

Figure 1. BACnet/IP network integration system configuration
The NAE85 allows integration of larger BACnet integration projects.
Important: From Release 13.0 and Releases 11.0 or earlier, the NAE85 can be either a Site Director or a child device to a Site Director. However, at Release 12.0 only, the NAE85 must be a Site Director and cannot be a child device. In the following configuration, an NAE85 can be used in place of the ADS/ADX Site Director, or as a child device reporting to the ADS/ADX Site Director.
Figure 2. NAE85 BACnet integration with NAE85 as child device