Syslog DDA - Metasys - LIT-12011832 - General System Information - Metasys System - 13.0.50

Metasys System Configuration Guide

Product
Building Automation Systems > Building Automation Systems > Metasys System
Document number
LIT-12011832
Version
13.0.50
Revision date
2024-12-02
Product status
Active

The Metasys system provides the optional capability of sending its configured audit log entries and alarm notifications to an external, industry-standard Syslog server, conforming to Internet published RFC 3164. The Syslog option provides positive indication of each field possible in the Metasys event and audit entries, replacing any blank field with the single character dash (-). Individual fields of each Metasys message are sent to the Syslog server separated by the vertical bar symbol (|), ensuring the integrity of all data sent to the Syslog server.

After the Syslog DDA is configured, all messages sent to the local ADS Repository are also sent immediately to the configured Syslog server. You can apply forensic analysis on the consolidation of all electronic audit and event information at the Syslog server.