Scheduling - Metasys - LIT-12011832 - General System Information - Metasys System - 13.0.50

Metasys System Configuration Guide

Product
Building Automation Systems > Building Automation Systems > Metasys System
Document type
Configuration Guide
Document number
LIT-12011832
Version
13.0.50
Revision date
2024-12-02
Product status
Active

Scheduling provides a graphical user interface that illustrates when events are scheduled to occur. Scheduling automates routine functions, such as transferring a room from occupied mode to unoccupied mode for heating and cooling needs, and energy optimization. Each schedule consists of a weekly schedule, an exception schedule, a list of items in the schedule, and an effective period. Exception schedules take precedence over the daily schedule only for their configured length and then return the schedule to its typical weekly schedule. Exceptions can include references to Calendars that can, for example, reflect a holiday schedule for the entire facility or show selected tenant spaces in the building. Another view within the schedule, called Today’s Schedule, shows the current day’s schedule including how each exception schedule affects the current day’s schedule.

A multi-time zone feature is available that allows the definition of schedules across different time zone. You can program schedules based on device time zones instead of converting the time to correlate to the Site Director's time zone.