Preferences - Metasys - LIT-12011832 - General System Information - Metasys System - 13.0.50

Metasys System Configuration Guide

Product
Building Automation Systems > Building Automation Systems > Metasys System
Document type
Configuration Guide
Document number
LIT-12011832
Version
13.0.50
Revision date
2024-12-02
Product status
Active
The Metasys system provides customized preferences for the Metasys user interfaces. The preferences allow you to configure how the user interfaces behave, including the sounds and colors, and alarm priorities. Preferences are divided into the following categories:
  • System preferences: apply to all users who log on to the site or device and affect the performance and operation of the system. In Metasys UI, you can set the system preferences through Site Settings.
  • User preferences: apply to a specific Metasys system user and define how information displays in the user interfaces. User preferences do not affect the operation of the system. In Metasys UI, you can set the user preferences through My Profile.