Logic Connector Tool (LCT) - Metasys - LIT-12011832 - General System Information - Metasys System - 13.0.50

Metasys System Configuration Guide

Product
Building Automation Systems > Building Automation Systems > Metasys System
Document number
LIT-12011832
Version
13.0.50
Revision date
2024-12-02
Product status
Active

Use the Logic Connector Tool (LCT) to create custom application programs that execute in any engine. The programs are created using a drag-and-drop editor. The programmer can connect real-time point data in the engine with logic blocks that perform mathematical, logical, and various specialized control functions. You can create, edit, and view LCT programs online through the Metasys UI or SMP UI, or offline through JCT or SCT.