Active Directory Federation Service (ADFS) two-factor authentication - Metasys - LIT-12011832 - General System Information - Metasys System - 13.0.50

Metasys System Configuration Guide

Product
Building Automation Systems > Building Automation Systems > Metasys System
Document number
LIT-12011832
Version
13.0.50
Revision date
2024-12-02
Product status
Active
ADFS integration with two-factor authentication is an add-on, licensed feature to add support for Metasys using ADFS, a single sign-on solution developed by Microsoft®. ADFS can then, in turn, be used to provide two-factor authentication for access to Metasys. ADFS helps prevent unauthorized access to Metasys, which, if not prevented, could result in data, financial, and reputational loss, system disruption, and other negative consequences.
Note: ADFS authentication is available to Metasys UI users, but is not available to Metasys SMP users. The ADFS single sign-on and two-factor authentication are configured on the customer's ADFS system.