Simplex Fire system - Metasys - LIT-12011832 - General System Information - Metasys System - 13.0.50

Metasys System Configuration Guide

Product
Building Automation Systems > Building Automation Systems > Metasys System
Document type
Configuration Guide
Document number
LIT-12011832
Version
13.0.50
Revision date
2024-12-02
Product status
Active
The Simplex Fire system includes a BACnet/IP integration, which facilitates the integration with Metasys. The Metasys system serves as a secondary fire monitoring system that can alert more people and automate building conditions when triggered by a fire event. The Metasys toolset is enhanced to simplify the workflow for integrating a Simplex Fire system:
  • The process of creating the Metasys Network, Equipment and Space integrations for SIMPLEX Fire Panels is automated through an updated Mass Change Tool utility in SCT.

  • There is a better representation of mapped fire system data in Metasys.

  • The Metasys UI provides a detailed view of the fire system components, and the exact location of the fire on the building and floor plan maps.