Modbus - Metasys - LIT-12011832 - General System Information - Metasys System - 13.0.50

Metasys System Configuration Guide

Product
Building Automation Systems > Building Automation Systems > Metasys System
Document type
Configuration Guide
Document number
LIT-12011832
Version
13.0.50
Revision date
2024-12-02
Product status
Active

Modbus is one of the most common communication protocols used in the industry. It is openly published and royalty-free, making it relatively easy to deploy for an industrial network. Modbus transmits raw bits, or words without placing many restrictions on vendors. Metasys Network engines support both Modbus RTU (RS-485, RS-232) and Modbus TCP/IP connectivity. The OAS uses the default network interface and supports Modbus TCP/IP only. For more information, refer to the Network Engine and Server Commissioning for Modbus Vendor Integration Application Note (LIT-12013150).