CWCVT Wireless MS/TP Converter - Metasys - LIT-12011832 - General System Information - Metasys System - 13.0.50

Metasys System Configuration Guide

Product name
Metasys System
Document type
Configuration Guide
Document number
LIT-12011832
Version
13.0.50
Revision date
2024-07-17
Product status
Active

The Connected Workflow Application Wireless MS/TP Converter (CWCVT) is a communications converter that provides a temporary wireless connection between a host device and equipment controllers that support the BACnet® MS/TP protocol.

The CWCVT is targeted for use by commissioning contractors and field technicians to efficiently perform commissioning and wiring validation functions for Metasys equipment controllers, TEC3000 Series Thermostats, and Smart Equipment Rooftop Units (RTUs). Through the CWCVT, the host device application can discover controllers connected to the MS/TP trunk, download applications, and commission the equipment. The CWCVT also supports a Wi-Fi wireless connection for Windows computers that run Johnson Controls® BAS Tools such as the Controller Configuration Tool (CCT), System Configuration Tool (SCT), or Applications and Parameters Loading Tool (APLT).