User Interface - Metasys - LIT-12011832 - General System Information - Metasys System - 12.0

Metasys System Configuration Guide

Product
Building Automation Systems > Building Automation Systems > Metasys System
Document number
LIT-12011832
Version
12.0
Revision date
2025-07-23
Product status
Active

Two variations of the user interface are available: Metasys UI and Site Management Portal (SMP).

The Metasys UI provides a simple location-based navigation approach to finding information, including the ability to search for any location by name and to bookmark a location in the browser. All data displayed in the Metasys UI is organized in a dashboard format, presenting to you the complete story of what is happening within a space, equipment, or central plant. You can access the Metasys UI from any type of client device with any screen size. The Metasys UI includes features ideal for efficient building operations.

For a comprehensive list of Metasys UI features refer to the Metasys UI Technical Bulletin (LIT-12012115) . For further details about individual features refer to the Metasys UI Help (LIT-12011953) .

Note: From Release 12.0, Metasys UI is also supported on the NAE85 and LCS85.

The Metasys SMP provides real-time and historical data views, extensive alarm management capabilities, and system configuration functions for system administrators or dedicated building operators. The SMP transforms the raw data from the site and organizes it into a comprehensive set of information management tools and reports. You can access this portal using the Launcher through an Internet or intranet connection to a Metasys server or engine. For further information about the SMP, refer to Metasys Site Management Portal Help (LIT-1201793) .

The following table describes the offerings at Release 12.0 and if they support Metasys UI, SMP with an add-on license, or SMP without an add-on license:
Table 1. Interface support at Release 12.0
ADX

ADS

ADS-Lite

OAS

NAE85

LCS85

SNE SNC NxE55xx-3 NxE55xx-2
Metasys UI X X X X        
SMP X 1 X1 X1 X1 X X X X
1 At Release 12.0, the SMP UI is a separate license available on this offering only to existing Metasys sites and to new or existing Metasys for Validated Environments (MVE) sites. If SMP UI is needed for this offering for an existing, non-MVE site, it must be purchased separately. For MVE sites, the SMP UI license is included with the MVE license and does not need to be purchased separately.