Open Application Server (OAS) system configuration - Metasys - LIT-12011832 - General System Information - Metasys System - 12.0

Metasys System Configuration Guide

Product
Building Automation Systems > Building Automation Systems > Metasys System
Document number
LIT-12011832
Version
12.0
Revision date
2025-07-23
Product status
Active

The OAS combines the functions of a Network Engine with a Metasys Server.

As a Site Director, the OAS Standard supports up to two supervisory devices, 200 field devices, and 20,000 objects using BACnet/IP and Remote Field Bus integrations. The OAS supports integration with the following devices and systems: C•CURE-victor, Modbus, M-Bus, KNX, and OPC Unified Architecture (UA).

The OAS provides the Site Management Portal (SMP) and Metasys User Interface (Metasys UI).

Figure 1. OAS system diagram