Multiple network engine system configuration with one network engine designated as the Site Director - Metasys - LIT-12011832 - General System Information - Metasys System - 12.0

Metasys System Configuration Guide

Product
Building Automation Systems > Building Automation Systems > Metasys System
Document number
LIT-12011832
Version
12.0
Revision date
2025-07-23
Product status
Active

To extend the capabilities of your system, add one or more additional network engines. In the following figure, one network engine designated as the Site Director provides the Site Management Portal to all devices on the site. This configuration supports up to four simultaneous users.

Note:
  • This configuration only provides long-term storage of data through the use of the Metasys Export Utility installed on a computer.
  • The NAE45-Lite can be partnered with other NAE45-Lite devices only. Additionally, the NAE45-Lite requires an ADS-Lite-A Site Director, and both of these are available in specific markets only.
  • Similarly, the SNE110Lx can be partnered with other SNE110Lx type network engines only. Additionally, the SNE110Lx requires an ADS-Lite-A Site Director, and both of these are available in specific markets only.
Figure 1. Multiple network engine system configuration with one network engine designated as the Site Director