BACnet/SC network system configuration - Metasys - LIT-12011832 - General System Information - Metasys System - 12.0

Metasys System Configuration Guide

Product
Building Automation Systems > Building Automation Systems > Metasys System
Document number
LIT-12011832
Version
12.0
Revision date
2025-07-23
Product status
Active

BACnet/SC uses a hub-and-spoke topology. The central Hub Function performs message forwarding for all broadcast messages and for point-to-point messages for devices that do not support more efficient direct connections. All Metasys devices support direct connections.

The following figure illustrates the normal scenario of the BACnet/SC network, where every node is connected to the Primary Hub.
Figure 1. Normal BACnet/SC network scenario
The following figure illustrates the failover scenario of the BACnet/SC network, where the Primary Hub is offline and nodes get re-routed to the Failover Hub.
Figure 2. Failover BACnet/SC network scenario

For more information about the BACnet/SC topology and BACnet/SC more generally, refer to BACnet/SC Workflow Technical Bulletin (LIT-12013959) .