Optimal Start - Metasys - LIT-12011832 - General System Information - Metasys System - 12.0

Metasys System Configuration Guide

Product
Building Automation Systems > Building Automation Systems > Metasys System
Document number
LIT-12011832
Version
12.0
Revision date
2025-07-23
Product status
Active

Optimal Start automatically determines the correct time to start HVAC systems to ensure the facility is ready for occupants at the scheduled time. It adjusts to seasonal variations and minimizes the energy used.

The generic standard object screens handle the Optimal Start/Stop object configuration and focus views. The object defines views for configuration and focus, and the generic screens interpret the views to display the proper fields to the users. Users do not need custom screens or handlers.